Part Number: LMX2582
Other Parts Discussed in Thread: LMX2491
Dear TI Technical Support Team,
I am currently developing a signal source based on the LMX2582 wideband frequency synthesizer, targeting an output frequency range of 2.4 GHz to 2.5 GHz. The design requires a continuous frequency sweep with a fixed 100 kHz step size. A critical requirement is that the RF output must remain uninterrupted throughout the entire frequency sweeping and switching process, with the instantaneous output frequency deviation strictly limited to a small margin relative to the current or next target frequency.
According to the LMX2582 datasheet, the VCO3 core has a native tuning range of 4481 MHz to 5092 MHz. Its subsequent divide-by-2 output path can fully cover the entire 2.4 GHz to 2.5 GHz target band.
I would greatly appreciate it if you could confirm whether the LMX2582 can fully satisfy these performance requirements. If feasible, could you also provide a step-by-step, register-level configuration procedure to implement this function properly?
Thank you for your assistance.