This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK01801: Model Selection

Part Number: LMK01801
Other Parts Discussed in Thread: LMK01000, LMK04906, LMK04828, LMK04832

Hi TI Experts,

In my application, a low-noise clock device is considered to divid 1GHz input signal to 100MHz output. I use only one output. Please assist to find a proper device that meets below items.

1, Best output phase noise at 100MHz. Ideally, spec

    -110dBc at 1Hz offset,  

    -120dBc at 10Hz offset,

    -130dBc at 100Hz offset,

    -155dBc at 1kHz offset,

    -165dBc at 10kHz offset. I understand this is hard to achieve, but I would like to know TI device has best close performance.

I looked into LMK01000, LMK01801, they have noise floor data at 100MHz with no more details, I like to have more data at 1Hz, 10Hz, 100Hz, 1kHz, 10kHz and 100kHz offsets at 100MHz frequency output.

I also looked into LMK04906, LMK04828 jiter cleaner, it should work in bypass-PLL mode, but I can nor find phase noise data for this mode.

I like to know, which device is the best fit for me.

2,  The output type (LVPECL/LVDS/LVCMOS) is nor critical for me, any type is acceptable as long as phase noise is better.

3,  SYNC fonction is required.

The Sync signal is devided from 1GHz input, that is, SYNC signal and input has constant phase offset. In my application, the LMK output 100MHz signal is desired to have constant phase offset (or delay) to SYNC signal whenever LMK device is powered off then on. 

I looked into some LMK01000/01801 device, whose SYNC signal is designed to sync all outputs within bank, no more information on output-to-sync delay. 

I like to know which model number is the best fit or close for my applcaion, and i like to have more detailed data on phase noise performance. Please advise. 

Thanks,

Terry

  • Hi Terry,

    You would not see a complete phase noise mask for a clock buffer and divider like you would see for synthesizers. It is always a flat line (fixed additive jitter across frequencies). When a clock is divided and/or distributed. For a buffer it additive jitter exclusively depends on the source. A constant jitter is added to the source and that is your final jitter number. For a division, it would also additionally depend on how much you are dividing the clock (Inversely proportional). If you can share the phase noise profile of the 1GHz source, we can find the right device.

    I am using PLLatinum Sim to check for LMK04832.Say if you use a source with the noise mask you mentioned. Below is how your phase noise numbers would look for 1GHz input to 100MHz output, the performance will be limited by the noise floor of -163dBc/Hz. You can either try it on PLLatinum sim once you get the phase noise mask of the source or share it with us to check.

    Thanks,

    Rishabh