Hello...
I am evaluating the LMK04002B using the EVB. In the National clock design tool I can put any frequency in the input and using the proper relationship in PLL1 (R and N counters) I got to "lock" with the input frequency, for example, using a 122.88 MHz VCXO in PLL1, putting 12.288 MHz in the input frequency and setting R=1 and N=10 I got to lock the VCXO. But in the board LMK04002BEVAL I cannot lock with this same frequencies... I just got to lock using 122.88MHz in the input (the same frequcny of default VCXO) and "relation" 1 to 1 in R and N counters. Why? Why I can configure any frequency in the designs tool, but i cannot do it in a real world, I mean, in the EVB?
in the quick start guide of the LMK04002BEVAL is written: ..."Connect a reference clock from a signal generator or other source. Exact frequency depends on programming. Default modes use a 122.88 MHz reference"...
I tried to configure other frequencies, but only lock with 122.88MHz.
thank you very much!