Other Parts Discussed in Thread: BQ32000
I am having difficulties sourcing a crystal with 12 pF load capacitance, including the reference KDS DMX-26S crystal. I would like to use either a 6 pF or a 12.5 pF crystal, are there any means to correct this difference in load capacitance with extra passive components on the crystal circuit? I suppose it is possible to use the calibration feature of the BQ32000 RTC to compensate for the clock slow down or speed up, but I'd like to know if it can be done in hardware as well.