Part Number: LMKDB1202
Hi,
Our signal path routes from the source oscillator (Figure 1) through your switch (Figure 2) and then to our own controller (SoC).
However, the current model provided by TI is separated into an input model (Figure 3) and an output model (Figure 4). If the source oscillator has jitter, how should the output be configured?
Alternatively, can the source jitter be ignored, and can you provide us with the maximum jitter parameters (PJamp/RJrms, Figure 5) for the output (Figure 4)?
Figure 1:
Figure 2:
Figure 3:
Figure 4:
Figure 5:
Thanks!
Jeff