Part Number: LMK5B33216
Hi All,
For LMK5B33216 with a 125 MHz differential reference input and OUT0 configured for 125 MHz using true ZDM, what is the maximum input-to-output propagation-delay variation over −40°C to +85°C after the initial fixed phase offset has been calibrated? Does the ±65 ps tDLY-VAR-ZDM specification apply when the external input/output are 125 MHz but are divided internally to a TDC rate ≤26 MHz?
Thanks for any assistance!
Regards,
John Madsen