CDCLVP111-SP: LVDS INPUT or LVPECL ONLY?

Part Number: CDCLVP111-SP

Hello,

We're trying to run an SI simulation and notice that the part specifies in the features section that it is LVDS input capable.  However, IBIS model only seems to have an LVPECL option.  Also, LVPECL input IBIS shows a VID of 200mV which doesn't seem consistent with the datasheet which specifies a VID(min) of 500mV.

Thanks.