Part Number: F29H85X-MCAL-SDK
Hi, I've configured interrupt for gpt channel 0 (continuous mode) in eb tresos without os isr and the interrupt is executing only once i've checked for the registers after starting the timer of gpt TIE bit of cputimer register0 is 1 but after one interrupt it is getting 0 i checked for disable interrupt func call also no where it is executing after gpt start timer,
i've attached the main.c
#define APP_GPT_CH0_INT_ID (6U)
#define APP_INT_PRIORITY_DEFAULT (255U)
#define APP_INT_THRESHOLD (20U)
#define APP_PIPE_LINK_OWNER (2U)
MCAL_LIB_INT_ISR(Gpt_Ch0Isr);
uint32 Gpt_InterruptCnt[GPT_CFG_MAX_CHANNELS] = {0U};
static void App_RegisterInterrupt(uint32 InterruptId, uint32 Priority, uint32 IsrAddress)
{
uint32 int_config_addr = PIPE_BASE + PIPE_O_INT_CONFIG(InterruptId);
uint32 int_link_owner_addr = PIPE_BASE + PIPE_O_INT_LINK_OWNER(InterruptId);
HWREG(int_link_owner_addr) = (HWREG(int_link_owner_addr) & 0xF0U) | APP_PIPE_LINK_OWNER;
HWREG(PIPE_BASE + PIPE_O_INT_VECT_ADDR(InterruptId)) = IsrAddress;
HWREG(int_config_addr) = (HWREG(int_config_addr) & ~PIPE_INT_CONFIG_PRI_LEVEL_M) | Priority;
HWREG(PIPE_BASE + PIPE_O_INT_CTL_L(InterruptId)) = PIPE_INT_CTL_L_EN;
}
static void App_InitBareMetalInterrupts(void)
{
MCAL_LIB_DINT;
HWREG(PIPE_BASE + PIPE_O_GLOBAL_EN) = PIPE_GLOBAL_EN_KEY;
HWREG(PIPE_BASE + PIPE_O_MMR_CLR) = 0x3U;
HWREG(PIPE_BASE + PIPE_O_MEM_INIT) = PIPE_MEM_INIT_KEY | 0x3U;
while (HWREG(PIPE_BASE + PIPE_O_MEM_INIT_STS) != 0x2U)
{
}
HWREG(PIPE_BASE + PIPE_O_INTSP) = APP_PIPE_LINK_OWNER;
HWREG(PIPE_BASE + PIPE_O_RTINT_THRESHOLD) = APP_INT_THRESHOLD;
HWREG(PIPE_BASE + PIPE_O_INT_GRP_MASK) = 0x00U;
App_RegisterInterrupt(APP_GPT_CH0_INT_ID, APP_INT_PRIORITY_DEFAULT, (uint32)Gpt_Ch0Isr);
HWREG(PIPE_BASE + PIPE_O_GLOBAL_EN) = 0x3U | PIPE_GLOBAL_EN_KEY;
MCAL_LIB_EINT;
}
/*main function */
int main(void)
{
Mcu_Init(NULL_PTR);
#if (STD_ON == MCU_CFG_INIT_CLOCK_API)
Mcu_InitClock(McuConf_McuClockSettingConfig_McuClockSettingConfig_Osc2);
while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) /* Get PLL status and check */
{
/* Wait until all enabled PLLs are locked */
}
#if(STD_OFF == MCU_CFG_NO_PLL)
Mcu_DistributePllClock();
#endif
#endif
Port_Init(NULL_PTR);
Gpt_Init(NULL_PTR);
App_InitBareMetalInterrupts();
/* Reset Counters */
Gpt_InterruptCnt[GPT_CHANNEL_0] = 0;
Dio_WriteChannel(DioConf_DioChannel_DioChannel_0, STD_LOW);
Gpt_EnableNotification(GPT_CHANNEL_0);
Gpt_StartTimer(GPT_CHANNEL_0, GPT_COUNT_VALUE_10MS);
// Time_Delay(33);
while(1)
{
}
// return 0;
}
/* Time delay*/
// int Time_Delay(float64 seconds)
// {
// McalLib_Delay(GPT_TIME_DELAY_PER_SECOND * seconds);
// return 0;
// }
/* GPT timer channel 0 notification function */
void Gpt_Notify_Func_0(void)
{
Gpt_InterruptCnt[GPT_CHANNEL_0]++;
Dio_FlipChannel(DioConf_DioChannel_DioChannel_0);
}