Part Number: LMK1C1104
Are there any chips that feature a single-ended clock buffer similar to the LMK1C1104, but deliver a minimum output swing exceeding 1.62 V under a 1.8 V power supply? Note that 0.8×1.8 V (VDD) equals 1.44 V, which is less than 1.62 V. The output voltage is required to be higher than 1.62 V, otherwise the device cannot operate normally.