Part Number: LMK00301
Other Parts Discussed in Thread: LMK00105
Dear Experts,
Recently, a client has a project that requires the use of LMK00301SQE/NOPB and LMK00105SQ/NOPB for clock synchronization among multiple devices. The specific connection diagram is as follows:

DSP requirements for input clock specifications:
(1) Level range: 1.26V-1.8V
(2) Required duty cycle range: 48%-52%
(3) The frequency deviation is preferably controlled within 10 ppm
(4) The clock frequency deviation of DSP among multiple service boards should be minimized
The customer currently has the following application-related questions that require consultation, and hopes to receive answers from experts.
1. After cascading LMK00301SQE, how are the device tPD and P2P skew superimposed? According to this scheme, what is the total skew upper limit of the entire clock chain? Will the channel skew and duty cycle distortion of LMK00105SQ input and output itself affect the duty cycle specifications of DSP?
2. Is there any recommended differential impedance, differential pair length tolerance, and equal length constraint for clock routing between different service boards for cross-backplane LVPECL transmission?
3. Is there a recommended configuration for LMK00105SQ power supply filtering, specifically a coupling scheme for LVPECL input and LVCMOS output? Does the 1.8V LVCMOS output terminal require series resistance matching to ensure that the output level falls within the DSP's required range.
4. The input and output of LMK00105SQ belong to cross-power domain conversion. Does the chip itself have power-on timing requirements? If the buffer is powered on earlier than the DSP, is there a risk of reverse leakage in the 1.8V clock output pin of LMK00105SQ when the DSP power supply is not powered on?
Thank you