Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

LMX2492: Wrong Register Value in Tic Pro for CPPOL

Part Number: LMX2492

Hi

I am using the LMX2492 and TicsPro to generate the register values of LMX2492 for my application.

The polarity of the charge pump CPPOL is configured in register 28 in bit 5.
Here is a screenshot from the datasheet.
image.png

I configured CPPOL in TicsPro as positive and TicsPro wrote register 28 with the hex value 0x1F.
0x1F in binary has Bit 5 = 0, but for the positive CPPOL it has to be 1.
CCPOL_positive.png

When I configure CPPOL negative in TicsPro, than TicsPro writes register 28 with the hex value 0x3F.
0x3F in binary has Bit 5 = 1, but for the negativeCPPOL it has to be 0.

CCPOL_negative.png

It looks like TicsPro is writing this register value wrong.

Can you confirm this or am I overlooking something?

Best regards

 

Joscha