Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

CDCE6214: Few question for CDCE6214 EEPROM programming

Part Number: CDCE6214

Hello Expert.

I create this thread for double check.

Here is operation mode for CDCE6214 :

 image.png

Q1 : If customer want to programming internal EEPROM of CDCE6214, we must let device swap into "fall-back mode", isn't? 

Q2 : fall-back mode default support I2C communication for EEPROM programming, isn't?

Q3 : REFSEL and HW_SW_CTRL should be both "boot strap" pin, and we need to set REFSEL = floating or HW_SW_CTRL = floating to swap into "fall back mode" when CDCE6214 power on, isn't? there is not tacking effect when change pin status in run time?

Q4 : What is default value (setting) for EEPROM?

Q5 : I think "serial interface mode" also support I2C access, but it can not R/W EEPROM, isn't?

Q6 : I think EEPROM R/W cycles (Programming/Erase Cycle, Endurance) shoulod be much higher than 10 times, isn't?

Q7 : I2C interface is working when REFSEL = Low & HW_SW_CTRL = High, isn't?

image.png

Q8 : If device operation in "fall back mode", that is mean EEPROM reading will by-pass when CDCE6214 power up. Base on this working status, EEPROM is not loaded by default and all the trim values will be silicon default. I think silicon default value is register default setting, isn't?

Ref. https://www.ti.com/lit/ug/snau247b/snau247b.pdf#page=29

 

Thank You.

Gibbs