Hi,
We’re currently having problems with the CDCE62005 not outputting the expected frequency correctly on our board.
The board is set up with a 25MHz crystal on AUX IN and configured to generate 100MHz on Output 0 and 150MHz on Output 3 (both LVDS).
However, the 150MHz output is either 150.533MHz (which exceeds our expected tolerance) or 149.994MHz (which is withn spec). No measurements have been made on the 100MHz output.
The device will lock to either of these frequencies and remain locked. This causes an issue if it locks at 150.533MHz (as measured on a timer/counter).
Recalibrating at this point does not correct the frequency deviation.
Register settings:
Reg0 = EB02_0320
Reg1 = 6884_0301
Reg2 = 6884_0302
Reg3 = EB84_0303
Reg4 = 6886_0314
Reg5 = 6000_8BF5
Reg6 = 80BE_02A6
Reg6cal = 84BE_02A6
Reg7 = 8D00_37F7
Reg8 = 0000_0000
This problem is not seen when using the CDCE62005 eval card and loading our register contents – recalibrating gives 149.987MHz consistently (which isn't the same, but is considered adequate)..
Can you advise please?
Thanks
Stuart