Other Parts Discussed in Thread: CDCEL913
We have a CDCEL913PW
powered with 1.8V throughout,
and feed with a 27MHz LVCMOS clock
One of the outputs feeds a processor main clock,
which will be used to program this CDCEL913
during first-time operation after manufacturing of the Board.
The un-programmed chip has a factory default setting
where the input stages are configured for XTAL operation.
To my great surprise it turned out the input stage of the CDCEL913
doesn't reliable clock when feed with a 1V8 LVCMOS signal,
when it is still in its factory default setting for XTAL operation.
This means we have a deadlock and can't first-time program the CDCEL913
after manufacturing. (where we would switch over to LVCMOS configuration)
I've troubles to understand this situation, that is
I can't imagine what sort of input stages have been used,
which won't clock in face of a full swing 1.8V rectangle.
I'd ask you to shed some light on this issue,
and I'd recommend to add a warning to the data-sheet concerning this issue.
Thanks