Other Parts Discussed in Thread: LMK03000
what is the operation temperature of LMK3000C?
it is very hot on my board and no PLL function appeared !
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lin,
The maximum temperature of this device is rated in the datasheet is an ambient temperature of +85.
We have also taken into consideration that the die temperature will heat up hotter when you turn on the device and the outputs. In other words, the internal die is rated to a higher temperature than +85.
We have also considered the possibility of locking the VCO at -40 C and letting the temperature drift to +85 without reprogramming.
If you are within the operating limits of the device, have you also considered the TCXO or whatever reference is driving it?
If this signal fails, then this will cause our device to lock.
For diagnostic purposes, you can look at the N and R dividers of the LMK03000 to see what the frequency the part thinks it sees at the VCO and TCXO.
Regards,
Dean
If the device is very hot and behavior is not as expected, then you might want to check a few basic things (in addition to what Dean suggested earlier):
Best regards,
Alan