This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM7005 PLL_LOCK

Other Parts Discussed in Thread: CDCM7005

Hello,
 
My customer has a question about PLL_LOCK pin.
 
When reference clock does not exist, does PLL LOCK detect circuit work?
 
For your reference, my customer's  register setting is as follows. 
Word0 BIT30 MANAUT = 0 : They are using Manual Reference Clock Selection and always using SEC_REF.
Word1 BIT29 ADLOCK = 1 : They select Analog PLL_LOCK.
Word3 BIT2/3 Lock Window = 11 : Cycle slip.
Word3 BIT4/5 Lock Cycles = 01 : 64.
Word3 BIT6 CSLIP = 0
 
And they are observing the followings.
When they disable reference clock input, PLL_LOCK pin goes low and stays low at most CDCM7005s.
But PLL_LOCK pin goes low once and goes high again few seconds after at some CDCM7005.
 
So, the customer would like to know if PLL_LOCK always work properly even if reference clock input is not available, stays always low.
 
Best regards,
 
K.Hirano