Other Parts Discussed in Thread: CDCE72010
I am now trying to use the CDCE72010EVM in order to use the CDCE72010 in my hardware design.
I have problem using the CDCE72010EVM.
1. From the schematic of CDCE72010EVM, it seems that the 4 external loop filters are configured for 491.52MHz VCO output frequency and 10MHz input frequency. Is that so? Could I change the VCO output frequency to some other value other than 491.25MHz or is it determined by the external loop filters?
2. I am not inputting any clock into PRI and SEC, yet I am getting some output from clock output 0. Is it due to VCXO output? What is the correct way to use the EVM? Must I input a clock reference in PRI or SEC and use VCXO to synchronize the output clock to the clock reference.
3. Could someone provide a ini file for me to understand how the EVM works. Eg. provide clock output like 100MHz, 66MHz and 312.5MHz using some input clock frequency.
Thanks.