Other Parts Discussed in Thread: NE556, TLC552, NE555
Hello
Do you have a application circuit about synchronize or phase shift the both ch of NE556?
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Pan-M,
I am not sure what you are asking. Can you draw the input and desired output signals to help me visualize?
Regards,
Ron Michallick
Ron
Our customer are trying to create a circuit of 2ch inverter pulse about 100KHz.
Regards,
PAN-M
Pan-M,
Do the outputs need to be 50% duty cycle?
What should the phase be betterment the two outputs?
If the rate is greater than 150kHz, then the TLC552 would be a better choice.
Regards,
Ron Michallick
Thank you for reply
Our customer changed specification.
NE555 only work free running, and the output is wired to FET High/Low driver.
So, this is closed.
Thanks and regards,
PAN-M