This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC110X

Guru 13485 points
  1. CDCLVC110x family – It is mentioned in the data sheet that the Tr and Tf should be between 1 to 4 nano Second. What will happen if there will be a deviation from these numbers?
  • Hi,

    if the tr,tf>4ns the CDCLVC11xx will be more sensible to noise and therefore the additive jitter could sense some increase. The increase of additive jitter really depends on the system condition: it can be negligible if the no crosstalk or supply noise is effecting the signal.

    if the tr,tf<1ns actually there will be no impact in the system, except that the signal can sense some additional reflection if the impedance lane is not accurately matched.

    Best regards,

    Leandro