This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005 and CDCE72010

Other Parts Discussed in Thread: CDCE62005, CDCE72010

Is there a clock programmer jig available to program the following clock synthesizer chips CDCE62005 and CDCE72010?

  • Hello Wenjun,

    the CDCE62005 can be programmed with this s/w: http://www.ti.com/litv/zip/scac105d

    the CDCE72010 can be programmed by using this s/w: http://www.ti.com/litv/zip/scac100

    both s/w can be used with the appropriate EVM.

    best regards,

    Julian

  • Hi,

    I would like to ask for a test jig hardware to program the 2 clock devices. The EVM solution implies that the clock device chip has to be soldered to the board.

    Or is it that I should replace the clock device chip with a socket (by desoldering the EVM clock chip and soldering the socket to replace it). So, whenever I needs to program a CDCE62005 chip, I shall put the chip into the socket and program it, then take it out and put it onto some other application board.