This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005 PLL Lock problem

Other Parts Discussed in Thread: CDCE62005

We have an issue with the CDCE62005. The problem is that we somtimes havent a pll lock after a power on cycle and because of this the output frequencies were not stable.  Our system consists of a C6672 DSP the CDCE62005 Clock generator which generates 100 MH, 200MHz, 250 MHZ, 100MHz and 100MHZ on its clock outs and a PIC microcontroller which makes the power sequencing for the DSP. We use a 25MHZ Crystal at the AUX Input.

The Register settings inside the CDCE62005 are:

0xeb060300,     //  0

0xeb860301,     //  1

0xeb840302,     //  2

0xeb060303,     //  3

0xeb060314,     //  4

0x00000b25,     //  5

0x120e03e6,     //  6

0xfdc1f9e7,     //  7

0x80009c98 };   //  8

We tried everything which we found in this forum, e.g adding the >100pF to the PowerDownN pin, adding a external loopback filter but nothing helps.

Any ideas what can help ?