This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock output relationship

Other Parts Discussed in Thread: CDCE925

I am going to use CDCE925 for 2 different clock output. I can see same reference clock and difference rate clock outputs.

I hope 2 different rate outputs were on sync. Is CECE925 correct solution for this requirement?

THX 

  • Hi Woojung,

    do you need to have a Pdiv values different from 1 for your different rate outputs? If this is the case you may experience some phase shift between the two outputs.

    Best regards,

    Leandro

  • Hi Leandro,

    Yes. I am going to use different Pdiv value for each output clock. Can I understand the 2 output were from 1 source but there are some phase shift because of Pdiv value?

    I am going to make PHASE LOCK with external logic. If the 2 outputs were from 1 source, I would get the phase lock after some time.

    Thanks.

    Woojung