Other Parts Discussed in Thread: CDCE62002EVM, CDCE62002
Hi all,
I am having problems using the CDCE62002EVM. I would like to set up the EVM and then program the CDCE62002 part number that I implemented in a project. I tried the GUI in two different computers, Windows XP 32 bits and Windows7. For the first computer, I installed the driver from this link http://www.ti.com/tool/cdce62002evm and for the Windows7 computer, I am using this link http://e2e.ti.com/support/clocks/m/videos__files/480594.aspx - 0880.Installer.zip.
At the beginning, I was able to connect with the computer - Windows XP and after some time, LED D25- DEVICE COM went off. At the same time, the driver appears as Unknown device. I have tried to uninstall and reinstall but it have not worked. I have checked the SW and it was ON mode. Although the problem is that I am not able to connect with the microprocessor - USB and not with the CDCE62002.
I have tried with Windows7 but I got the same issue. The LED 25 is down. LED 26 brights so the chip is power up. This issue happens in three different boards that we bought.. I do not what I should do at this point because I think I have tried everything already.
I read that there was another person with a similar issue http://e2e.ti.com/support/clocks/f/48/t/183453.aspx. I am worried that something happened with the EEPROM when I tried to write the EEPROM unlocked through the GUI. The CDCE62002EVM uses the TUSB3210. I downloaded the TI USB EEPROM Burner Utility for the TUSB2136/TUSB3210 tool. When I tried to install it in Windows7 I got a issue - (eepromburnerDIg)(OnInitDialog)RegisterForDeviceNotification Fail (Error 13) and I am not able to select the TI USB device in the dialog box. Although I do not if this would solve my issue.
I hope a TI Guru can help me. Thanks in advance,
Victor