Hello,
I bought a CDCE913PERF-EVM Evaluation module.
It was delivered with a CDROM corresponding to an old EVM Evaluation board (with National LabView runtime), not that I bought.
I downloaded SCAC119c.EXE from this site and installed it.
TiClockPro start correctly, recognizes the evaluation board "CDCE913/CDCEL913(1)", (the light is green after I clicked the "Refresh" button in the second window) , but when I click on the "OK" button, the main window (displaying the registers) opens briefly and closes.
I have tried installation on several PCs (Windows 32 bits or 64 bits) but the problem is the same : TiClockPro close immediatly.
Why is wrong ?
Thank you.