Other Parts Discussed in Thread: CDCE72010
Hi,
I am trying to configure a CDCE72010 for using an external reference clock of 10 MHz (coming from instrumentation) connected to SEC_REF. It also uses a 491.52 MHz VCXO for clock generation. The register values are the following:
682C0290
68000021
83800002
68000003
E9800004
68000005
68000006
83400017
68000098
68000049
0BFC07CA
8000040B
0000180C
Charge pump current = 2.2 mA
R = 1 , N = 125, M = 768 and P = 8
The PLL filter is configured as:
C1: 100nF
R2: 4k7
C2: 22uF
R3: 160ohms
C3: 100nF
The PLL does not lock. The excel loop filter simulator gives a closed loop bandwidth of 67 Hz for an update frequency of 80 kHz.
Is something wrong?
Thanks in advance