This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK4906 EVB, VCXO oscillator ref ?

hello

On the LMK4906 EVB instruction, the shematics part number of the 122.88Mhz VCXO is CVHD-950-122.88. There are clearly six pin on this oscillator, but on the datasheet of the CVHD-950  as only 4 pins!   (http://www.crystek.com/crystal/spec-sheets/vcxo/CVHD-950.pdf)

is there a error in the shematic reference ?

Thanks,