Other Parts Discussed in Thread: CDCE62005, CDCM6208
Hi,
We require two output frequencies for our application - 110MHz and 200MHz. Can they be simultaneously generated by the device? To achieve these frequencies, the output from prescaler must be 2200MHz which is the LCD of 110MHz and 200MHz. It however does not look possible from the device as prescaler has minimal divide ratio of 2 and hence we may need to get VCO output of 4400MHz.
Is there any software tool available for simulating the register values or can TI help on register values for these two frequencies? Our reference input is at 25MHz.