Other Parts Discussed in Thread: CDCM6208
In CDCM6208 datasheet it is mentioned that, while using this device to clock ADC, there will be SNR degradation when the IF frequency is above 100MHz. Our IF is around 160MHz. Is it recommendable to use CDCM6208 in this case? Or is the SNR degradation common for all clock generators? We need to provide 110MHz clock to ADC.