Other Parts Discussed in Thread: LMK00101
Hi,
From the datasheet I see that:"If the DC coupled input swing has a common mode level near the devices internal bias of 1.4 V, then only a 0.1 μF bypass cap is required on CLKinX*. Otherwise, if the input swing is not optimally centered near the internal bias voltage (of 1.4), then CLKinX* should be externally biased to the midpoint voltage of the input swing"
My OCXO is:"The CMOS output swings from rail to rail – the average DC level is 1.65V for 3.3V supply"
Is this Voltage is "near the devices internal bias of 1.4 V"?
What is the Recommendations for this issue?
Thanks