Other Parts Discussed in Thread: LMX2531
Hi, dear all,
I met a problem with PLL 'LMX2531LQ1500'. I have two same boards with a PLL and clock buffer on them and the PLL and clock are all configured by FPGA. The PLL in the first board is working well. When the second board came, we use the same FPGA codes and we test the clock input, LE and CE all meet requirements, but there is no output. So we thought may be some thing wrong with the PLL chip and replaced it by a new one. But it's still the same thing. Also we cut off the output(to clock buffer) and extend the output to ground with a 49(Ohm) resistor, there is still no output.
(Further, the two PCB boards have the same layout but produced by different PCB companies. I do not think it would make any difference)
We can not figure out other ideas to fix this, can you kindly give some advice?
Thanks so much!
Su