Hello,
Due to the availability of the new LMK National/TI clocks with very good performance we consider to change our previous direct RF DAC design because they match near exactly to our dual PLL loop topology, as you will check below, and we will save a lot of circuitry making the HW design extremely compact.
Our clock is composed of 3 blocks, a first 10 MHz basic block which is external to the design and have different implementations depending on the transmission system, an intermediate PLL block at 70 MHz using a Crystek VCXO (very close to the examples in the LMK04XXX data sheet), and a final RF DAC clock at a frequency in the range of 2.2 to 2.4GHz.
The predesigned clock frequency and the preliminary DAC tests were performed at the 2.31 GHz frequency (2310 MHz).
As we need only 3 or 4 frequencies as outputs (for DAC, FPGA and test), we consider first the use of the LMK04906, that a bit confusingly for me is announced somewhere as covering the range 2.26 to 2.6GHz.
Reading the data sheet we discovered that the real device range is 2.37 to 2.6GHz so our initial 2.31GHz frequency could not be feasible using this chip.
We considered then to move our clock to the next 70 MHz multiple i.e. 2.38 GHz. No clock or DAC test have been done using this value but we don’t envisage any problem. Nevertheless, we discovered later using selection tables that there is a whole other family LMK048XX that include several chips, one of them covering exactly the same range than the LMK04906, but other in the family (LMK04805) being able to work at 2.31 GHz. They have nevertheless many outputs that we don’t need and is a bit more expensive.
On the other hand, we have a general question related to the suitability fof all these families when what you need first of all is to extract a differential, ultralow jitter 2.3GHz clock, not divided outputs as in the examples (for example the device jitter is specified only about 200 MHz, even if the clock jitter must be roughly constant with frequency when measured in time)
1) Do you recommend LMK048XX and LMK049XX for this application, where we need a physical 2.31 or 2.38GHz differential output, not divided outputs in the 100’s of MHz ranges?
2) In case the reply to 1) was yes, in order to get the best clock jitter what would you recommend us, to use the LMK04906 at 2.38GHz, theLMK04806 at 2.38GHz or the LMK04805 at 2.31GHz? And as it seems logic that one day we will have the LMK04905, it can be added it to the chances list.
A factor that can help or complicate the reply is that when the output is multiple of twice the 70 MHz primary PLL reference, we can use the internal chip doubler, getting normally a better jitter. This advantage would only be available when using the 2.38GHz output, ither with LMK048 0r 049 I guess.
As I understand, as we need less than 6 outputs the most economic is to use the LMK049XX family. But then it comes the exact frequency issue.
Thank you very much in advance
Jaime Martin