This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1GX04DRLR

Hello,

I am trying to generate a square wave ate 13.56MHz using the SN74LVC1GX04DRLR oscillator driver.

1) First a calculate the values of the caps. According to the datasheet : 

CL = (C1*C2) / (C1+C2)  and C1 = C2.  My oscillator has CL = 18pF. Therefore, I have C1 = C2 = 36pF.

2) Then, I calculate the value of Rs. Again, according to the datasheet :

Rs = Xc2 = 1/ (13.56MHz * 36pF * 2 * pi) = 326ohm.

3) Finally, I chose for Rf the same value as in the datasheet : 12Momh.

I made a PCB, with ground plane under the oscillator and soldered everything (and double checked). 

It seems like the oscillaiton does not start.

Any idea?

thanks,