Other Parts Discussed in Thread: CDCM61001
Hi,
Please teach about the required specifications for input X'tal to CDCM61001.
In the data sheet are required a drive level as max 1mW.
On the other hand, two are max 500uW in three recommended X'tal in the datasheet. And one is like max 100uW.
X'tal which max 1mW can permit is not common.
Please teach the true maximum Drive Level required to X'tal.
Best Regards