Other Parts Discussed in Thread: CLOCKDESIGNTOOL, LMK04816
Sir:
I need do a design of time-interleaved ADCs of 14bit, so the time tree must be in high performance. The new generation low noise PLL of LMK048** and LMK049** attract my attention. After read the datasheet of these devices, I still have some doubts about the feature and the application.
(1) the datasheet give the jitter performance is about 100fs for LMK048**. Is it the parameter of JITTERadd?
(2) LMK048** can be used in dual PLL mode and single PLL mode, which mode has better performance? In which mode was the device tested to get the jitter performance of 100fs.
(3) If I want to use the device in dual pll mode, how do I construct the external loop filter?
Jacky
thx