Other Parts Discussed in Thread: LMK04906
TI Team,
I plan to use the LMK04906 and I have a couple of questions regarding its operation.
I'd like the ability to bypass the VCO and output the VCXO clock, or another external clock, under some conditions. There are two methods I see to accomplish this. First, CLKOUT3 and CLKOUT4 appear to have OSCIN muxes which I can use. Second, CLKIN1/Fin appears to allow direct distribution of the input clock to the outputs. Can I loop back OSCOUT to CLKIN1/Fin and disable the 1st charge pump to output the VCXO clock to all outputs?
Can this be done? Is this not recommended for any reason?
-David