Other Parts Discussed in Thread: LMK04906, CLOCKDESIGNTOOL, LMK02002
sir:
My clock generator produce 4 channel clocks with the frequency 250M~400MHz, and each channel pass through a VCDL(voltage control delay line). But when the clock pass through the VCDL, the phase noise increase, with the RMS jitter about 400fs(12KHz~20MHz). I search for a simple jitter cleaner, which can filter the phase noise of each clock. I hope the jitter cleaner can produce a clock with RMS jitter below 100fs.
Is there some device that meet my requirement?
Thank you!
Jacky
2013-06-05