Other Parts Discussed in Thread: CDCE937
Hello,
Please answer my customer's problem.
Power up sequence of customer's board is VDDOUT(3.3V) ON first and VDD(1.8V) ON next.
EEPROM is Factory Default Settings as explained in Table 4. of datasheet and S0 is set LOW, so customer expects Yn output are Hi-z until S0 is changed to HIGH.
But Yn output High level until VDD(1.8V) is ON (between 3.3V ON and 1.8V ON period).
Q1: Are their any requirement of power up sequence?
Q2: Yn must be Hi-z after 3.3V is ON in their system.
Are their any countermeasure to keep Hi-z after 3.3V is ON?
Regards.