Other Parts Discussed in Thread: LMK04828
Hi,
I am starting a design and wanted to ask for feedback on the LMK04828 clock jitter cleaner and distributor. The aim is to generate 8 trigger signals from the sysref output clocks (one output will have a fanout buffer to generate the 8th signal). The requirements include:
- The sync outputs should be able to multplex between: external sync input, onboard 1pps from GPS module, FMC sourced sync
- The sync should be resynchronised to the generated clock after multiplexing
- It should be possible to lock the clock to a 1pps pulse.
- It should be possible to shift each sync with 1/4 clock cycle resolution (ie 90,180,270 )
Clkin1 on the device is driven by a clock source that we would like to sync our trigger signals to. Figure 5-2 in the datasheet implies that this is possible. The frequency of clkin1 will be approximately 2.5GHz. Clkin0 will be driven by an external trigger signal to drive our trigger/sysref outputs. The sync pin will also have inputs from a locally generated 1 pulse per second signal or a sync signal sent from an external FPGA. From what I understand, the sync pin can also drive the sysref outputs if we require it?
Do you know the availability/status of the LMK04828 part? I have tried to source it from several suppliers but it currently has a minimum of 6 weeks lead time from some suppliers. Do you anticipate any issues with sourcing this part for the future?
Also, from my requirements, does it seem to be the best solution available from TI do you think?
Best Regards,
Fearghal