Other Parts Discussed in Thread: CDCE72010
Hi all,
I just bought a CDCE72010EVM evaluation module for the CDCE72010 device.
I need to generate an LVCMOS output between 0 V and 3.3 V (or at least 0-1.5 V) to clock a design implemented in an Actel ProASIC3 FPGA, on a commercial board (ProAsic3 Evaluation Board).
How shall I do?
I can only generate LVCMOS outputs between -800 mV and +960 mV (with a divider of 80).
I use USB to power up the evaluation module and, if I try external 3.3V power, I cannot generate any clock.
So, I enable 'EVM power' in the control GUI, select USB power on the board and select, by the control GUI, LVCMOS level on output 2 with a divider of 4'. The other parameters are default. I get a clock of about 120 MHz between -440 mV and 520 mV.
If you need more information about my test I'm ready to provide anything, only I need to know what ;-)
Thank you in advance!
Niccolo`