Other Parts Discussed in Thread: CDCE72010
Hi there!
I have a PCB with a CDCE72010 clock synchronizer on it but the SPI communication doesn't work. Probably i do something wrong on the master side or the hardware desing is faulty but i can't figure out what could be the problem. General troubleshooting steps have been done (check power pins, check signal levels etc) and the ic have been replaced once also.
Here are oscilloscope screenshots from three consecutive read requests: (signals are LE, MISO, MOSI, SCK)


I issue a read command with 1110 (zero first) followed by the address 1100 and 24 0s. Than i pulse LE and send 32 clock pulses for incomind data. Can anyone tell me whats wrong with this?
It might be simple but i'm working on it now for more than a week and i'm really tired of it. Any help would be highly appreciated.
Thank you!