This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the input of LMX2581.

Guru 19645 points
Other Parts Discussed in Thread: LMK01010, LMK01020, LMK01000, CDCM1802, CDCE18005, CDCP1803

When 80-MHz carrying out a differential clock output, which shall be used between OSCin and Fin from a 640-MHz clock input?

If 640 MHz is put into Fin and an output divider is set as one eighth, I will think that an 80-MHz differential clock is outputted, but how to use OSCin at that time and Vtune is not known.

Please teach me a solution.

Thank you for your consideration.

  • Hi Satoshi,

    If you want to get a 80MHz differential clock output from a 640MHz clock input, I suggest use clock buffer instead of PLL synthesizer.

    For example, LMK01000, LMK01010, LMK01020, CDCE18005, CDCM1802, CECM1804, CDCP1803. These clock buffers all have built-in divider.