This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04803B / current consumption calculation

Guru 20090 points
Hello,
 
I calculated below conditions current consumption by LMK04800 datasheet page 121~121.
Is below my calculation correct ?
If not, please let me know correct calculation.
 
<Conditions>
Dual loop mode
2 LVDS with 250MHz (CLKout0 and CLKout1)
1 LVDS with 2GHz (CLKout2)
No other features enable
 
<Calculations>
Core : 140mA
Base Clock Distribution ; 17.3mA
Clock Divider / Digital Delay : 25.5mA * 2 = 51mA
LVDS : 14.3mA *3 = 42.9mA
-----------------------------------------------------
Total : 251.2mA
 
 
Best Regards,
Ryuji Asaka