This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0041 + LMH1983 Synchronization

Other Parts Discussed in Thread: LMH0041, LMH1983

Hello,

Our aim is to generate 3 frequencies synchronized with SDI video clock provided by a LMH0041.

The 3 frequencies are :

  • 74.25MHz                  27Mhz   12.288MHz
  • or
  • 74.25MHz/1,001      27MHz       12.288Mhz
The LMH0041 is provide a recovered clock from SDI (SD:27MHz   HD:74.25x2  or 74.25x2/1,001). We plan to extract F/H/V signal from SDI stream (after the LMH0041) into a FPGA  and provide them to LMH1983.
Is there any reference design related to this topic?
Is there any timing specifications about the F/H/V inputs of LMH1983? (H min pulse width, V timing relation with H, etc...). 
Thanks in advance.