I'm switching from an XP computer to a new Win7 64 bit computer. I installed a Rosewill parallel port card to program my devices. Since the card is not LPT1, 2, or 3, I enter the cards address (from Device Manager) into the "Other" box (the address range is D010-D017, and either give the error). When I do so, I get "Run-time error '6': Overflow"
What could be causing this, and is there a possible remedy? I've already seemingly exhausted trying to make the card act like LPT1. BIOS won't let me assign it that address.