Other Parts Discussed in Thread: TPL5000
I'm wondering if someone can set me straight and confirm or correct my design. I have the TPL5000 chip. I'm making a breakout board just to test in another circuit. I'm connecting D0,D1,D2,VDD and PGOOD all together and to 3.3V. I'm connecting DONE and GND to 0V. RSTn and TCAL are floating because I'm not interested in that right now. I'm expecting WAKE to get toggled on and then off every 64s. I'm not seeing any movement on the WAKE pin at all. Any ideas? Am I expecting the wrong thing, or must there be something wrong with my circuit/observations.
Thanks