This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI Part suggestion for System Clock level translation

Other Parts Discussed in Thread: LMK00105

Hi,

I"m getting System clock from the base board to clock the FPGA in my daughter card. The system clock is ~166MHz with voltage level of 1.8V or 3.3V (programmable in base board). I need to interface this SYSCLK to GCLK of FPGA port which will have VCCIO voltage of either 1.8V or 2.5V or 3.3V (programmable, supply from base board).

Please suggest a TI device to support all possible level translation combination from VDD1(1.8V/3.3V) to VDD2(1.8V/2.5V/3.3V) without delay.

Kindly check & suggest TI part ASAP.

Thank you.