Hello,
My customer have a question about LMK00105.
The conditions of the customer as follows.
[Conditions]
CLKin / CLKin* = LVDS, DC Coupling input
VDD = 3.3V
[Q]
When the state of the LVDS source is Tri-State, the noises occurs from the outputs of LMK00105 in the customer board.
I attached an example.
This is not the periodic noises.
In this case, the states of CLKin and CLKin* looked Logic High.
Please teach me what is considered as a cause of the noises.
Regards,
Hiroshi Katsunaga