This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM7005 power-up default settings

Hi, 

I'm reading the data sheet but having a hard time understanding it. After the device powers up or comes up from PD, what is the value of the Yx_MUX registers? i.e. What P-divider value will be routed to the output buffers?

The data sheet table on pages 24-25 indicates that the default is Yx_MUX[2:0]= "101" which would lead to "Div-by-8" being the default, but right under the table theres a footnote saying: "In the default mode (after power up), Div-by-16 is selected"

Which is it?