This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Asaka-San,
LMK03806 can generate 304 MHz from an off-the-shelf 16 MHz crystal oscillator with ~200fs RMS jitter (12 kHz - 20 MHz). LMK04906 (in single PLL configuration) is another option if you preffered to have fewer outputs. However, these devices do require Microwire programming to achieve the desired output frequency
CDCE62002 can generate the required frequency with a 38 MHz oscillator with ~300fs RMS Jitter (12 kHz - 20 MHz) but it requires a write to the EEPROM
For high volume applications, we can also support ROM spins our devices to address the required frequencies on power-up. I will notify the marketing enginner to follow up with you on the opportunity size / design timeframe.
Couple of follow up questions:
1) How many copies of the output frequency would you like? Are there other frequency requirements in your system?
2) Where is the 304 MHz clock used in your system?
3) What is the phase noise integration bandwidth for the jitter?
Regards
Arvind Sridhar
Hi Asaka-San,
Thanks for the reply. I do not have further information to add to my previous email.
Regards
Arvind Sridhar