Hello from Sydney Australia!
I have tried a circuit that 'Ramps' eight traces on a single channel CRO.
I have tested it and it 'Strobes' 4 traces quite well but 8 traces looks to be a little harder.
Without trial and error ,in theory how do you work out the Clock Frequency needed to display the
full 8 traces at about 10-25 frames per second without noticeable 'flicker'?
It is a Digital Cro , and therefore the need for a variable Clock as the Digital Cro's don't seem to
have a Variable Time Base.
In order to continue pursuing this circuit the Display part of the circuit has to work first.
If it is 'Out of Sync' with the 'Test Circuit' a 'Memory Buffer' will sort out this problem , even if it doesn't
display it in 'Real Time'.
Thankyou-Simon